AXIS#.PL.KFB.POUT

Please refer to AXIS#.PL.KFB.PIN for details.

Versions

Action Version Notes
Implemented 02-08-01-000  

General Information

Type Read/Write
Units N/A
Range 1 to 2,147,483,647
Default Value 1
Data Type Integer
See Also AXIS#.PL.KFB, AXIS#.PL.KFB.PIN, AXIS#.VL.KFB
Stored in Non Volatile Memory Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.PL.KFB.POUT

500ch

12h

Signed32

-

-

Read/Write

No

AXIS2.PL.KFB.POUT

510ch

12h

Signed32

-

-

Read/Write

No